AXIS#.VL.AINACC

Description

Defines the acceleration ramp when the axis is in Analog Command Source, and Velocity Mode.


  • This keyword has no effect when the drive is in Torque or Position mode.

Versions

Action Version Notes
Implemented 02-01-02-000

General Information

Type

Read/Write

Description Describes the acceleration ramp for the velocity loop.
Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

Linear: counts/s2, mm/s2, µm/s2, (custom units)/s2

See Acceleration Units for details.

Range

Depends on units. See Acceleration Units for details.

Default Value

10,000 RPM/s

Depends on units. See Acceleration Units for details.

Data Type

Float
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
AXIS1.VL.AINACC

5011h

21h

Unsigned32

Acceleration 16Khz

-

Read/Write

No

AXIS2.VL.AINACC

5111h

21h

Unsigned32

Acceleration 16Khz

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.AINACC

6038

1796

Signed32

Read/Write

Acceleration

AXIS2.VL.AINACC

71574

1179

Signed32

Read/Write

Acceleration

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.AINACC

6038

Float

Read/Write

Acceleration